Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Are Schneider Electric Altivar drives 6, 9, 12, 18 or 24-pulse?
Issue:
Are Schneider Electric Altivar drives 6, 9, 12, 18 or 24-pulse?

Product line:
Altivar 61 71 12 312 212 320 32 630 650 930 950

Environment:
All models, all serial numbers

Resolution:
Schneider Electric Altivar VFDs are 6-pulse.  The enclosed Power Guard product, which is currently obsolete was 18-pulse.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)