Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the mean time before failure for the ATV61HD15Y?
Issue:
ATV61HD15Y Mean time to failure

Product line:
Altivar 61

Environment:
ATV61HD15Y

Cause:
What if the life expectancy of the ATV61HD15Y?

Resolution:
The average time before failure (MTTF, Mean Time To Failure) is 350,000h for ATV61HD15Y.
The MTTF take into account the electronic boards and the power components. The fans are not taken into account for the calculation of the MTTF.