Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Is there a baying kit or bracket to connect a NetShelter SX to a VX?

Issue:
Customer has SX and VX cabinets installed side by side.

Product Line:
NetShelter SX, NetShelter VX

Environment:
All versions and serial ranges.

Cause:
Customer wants to use baying brackets to align the cabinets.

Resolution:
There are no baying brackets or kit which allow a SX cabinet to bay to a VX cabinet.