Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How much internal meter memory is available for data logs on the PM5300 & PM5500 models?
Issue
Would like to know the internal meter memory capacity available for data logs of the PowerLogic PM5300 & PM5500 models.

Product Line

PM55xx

Environment
Memory

Resolution
The memory capacity of data logging available for PowerLogic PM53x0 & PM55xx models is 256 kB & 1.1 MB respectively.

Note: These meters use a single data log and have a separate alarm logs which holds up to 40 entries at a time.