Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the ATS22 adjustment range for parameter In, Motor Rated Current?

Issue:
Motor Rated Current adjustment range on the ATS22.

Product Line:
Altistart 22 ATS22

Environment:
All models

Cause:
What range of motors can be used for a particular ATS22 model

Resolution:
The Motor Rated Current, In, is adjustable from .4x to 1.0x the ATS22 current rating, IcL.
In other words, it can be adjusted down to 40% of the ATS22's rating.

Eg: An ATS22C17S6U, rated 170A, has an In range of 68 - 170A.