Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Is there a way to control where the popup panel will open in Vijeo Designer?
Issue:
Looking for a way to program a popup panel in Vijeo Designer to open at an exact co-ordinate.

Product Line:
Vijeo Designer

Resolution:
It is possible to specify a switch object to open a popup window at the X,Y coordinates of where you want the popup panel to open.  That option is in the switch's Popup panel operation. Please see the example below to specify to open the popup window at (0,0) --> Top left of the screen.
Switch Settings