Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Power Monitoring Expert - Alarms and Events not updating on remote Web Clients

Issue:

The Alarms Tab in the PME Web Applications is not updating with new Alarms and Events. The Updating indicator continues to operate which suggests the Alarms Tab is updating, but nothing new is displayed.
Product Line:

Struxureware Power Monitoring 7.0(SPM)

Power Monitoring Expert 7.2.x

Power Monitoring Expert 8.x

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment:
Web Applications
Alarm Tab
Cause:
The Web Clients do not dynamically reconnect to the server if there is a connection loss between the remote machine and the Primary Server. If the Primary Server is rebooted or the services restarted, the Web Clients will lose connection and will not reconnect.
Resolution:
If the Primary Server is rebooted or the ION Services are restarted, all Web Clients will need to be logged out and logged back in to resume normal operation.