Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
My M221 (or M241 or M251) is connected by USB and it does not answer at address 90.0.0.1…
This is a normal behavior: previous controllers as ATV IMC or M258 were seen as modems by Windows, with IP address 90.0.0.1.

This is not the case of M221, M241 and M251: they are seen as generic USB devices and they do not have an IP address when connected via USB.