Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How can I see the last faults that occurred on an ATV61 or ATV71 drive?

Issue:
ATV61/ATV71 last faults

Product Line:
ALTIVAR 71 ATV71 ATV61 Altivar 61

Environment:
All

Cause:
Faults

Resolution:
Go to menu 1.10 Diagnostics then to Fault History.
Faults are listed most recent to oldest.
You can highlight and press enter on each fault to confirm a number of things that registered at the time of fault.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)