Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What causes Concept error "open Pin expected wrong scope in pin array "?
Issue:
Error message is displayed when importing a Concept .ASC file.

Product Line:
Concept Programming software

Resolution:
This is usually caused by a corrupt or incomplete .ASC file.   Make sure that the .ASC file ends with a 'CR_END *'  statement.
You may have to re-export the Concept project to produce a good and complete .ASC file.