Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the part number for the remote keypad for the ATV312 variable speed drive?

Article available in these languages: Španělština

Issue:
Remote keypad options ATV312

Product Line:
Altivar ATV312

Environment:
All models

Cause:
Needs to get keypad for the ATV312 drive.

Resolution:
There are three keypad options for the ATV312 drives.

Option 1:
Graphic LCD display keypad ( ATV61/71 keypad can be used with the ATV312 drive)
VW3A1101 is the HMI keypad
VW3A1102 is a remote mounting kit with bezel providing IP54
VW3A1103 is an optional cover to provide IP65

A remote cable is offered in various lengths:
VW3A1104R10 is 1 meter
VW3A1104R30 is 3 meter
VW3A1104R50 is 5 meter
VW3A1104R100 is 10 meter

Option 2:
VW3A1006 is a standard LED keypad rated IP54
VW3A1104R** cable same as option 1 above

Option 3
VW3A1007 is a standard LED keypad rated IP65
VW3A1104R** cable same as option 1 above