Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
When was the LH4N soft start line made obsolete?
Issue:
Customer wants to know when the LH4N soft starts became obsolete

Product line:
LH4, LH4N

Environment:
All models

Cause:
Obsolete

Resolution:
The LH4N became obsolete in January 2005.  The current replacement product for form, fit and function is the ATS01 soft start series.  Customers should still review the product ratings and dimensions before ordering.
The Installation Manuals for the LH4N and the ATS01 are attached.

Schneider Electric Česká republika

Přílohy
LH4N Soft Starter Installation Manual.pdf [143.1 KB]
ATS01 installation manual.pdf [1.99 MB]