Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
When did the ATS23 soft start become obsolete?
Issue:
Is the ATS23 obsolete?

Product Line:
ATS23

Environment:
All

Cause:
N/A

Resolution:
ATS23 became obsolete in August of 2003.  The current replacement is the ATS48.  There are some differences that should be reviewed by the customer such as wiring, dimensions and ratings.