Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the I/O scanning health bit address for a M340 NOE module.
Issue:
I/O scanning health bit address for a M340 NOE module.


Product Line:
M340 PLC


Resolution:
If a BMX NOE 01x0 module is configured in rack 0, slot 3, the health bit address would be as follow:

%IW0.3.0.1    device 1 - 15
%IW0.3.0.2    device 16 - 31
%IW0.3.0.3    device 32 - 47
%IW0.3.0.4    device 48 - 64