Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Will the PM5000 series meter change the energy units on the display after exceeding 1000 GWh?
Issue
The PM5000 series meter has accumulated over 1000 GWh of energy, user wants to know if the display with change units to TWh automatically.

Product
PM5000 series meter

Environment
PM5000 with high energy use

Cause
The units for energy consumption is automatically adjusted as energy is consumed

Resolution
The PM5000 meter will automatically change from GWh to TWh.