Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How to determine which option cards are installed on the ATV61 and 71 VFDs?
Issue:
Which option cards are installed on the ATV61 and 71 VFDs?

Product Line:
ALTIVAR 61, ALTIVAR 71,

Environment:
All drives all serial number

Cause:
N/A

Resolution :
To verify what options cards are installed on the Altivar 61 or the Altivar 71 VFD you can do the following:
Drive menu - Press enter
Identification Sub Menu -  Press enter
Scroll to Option 1 and Option 2, there the two options will display the option cards installed on the VFDs