Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What can cause an internal link fault on an ATS22 soft start?
Issue:
Possible cause for an internal link fault on an ATS22 soft start.

Product Line:
ATS22 Soft Start

Environment:
All models and serial numbers

Cause:
Internal detected fault

Resolution:
Internal serial link fault means the soft starter control card is not communicated with the power board.   Try reseating the ribbon cable that connects the control card to the power board.   If this does not resolve the issue, repairs or replaces the soft start.