Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Can Unity Pro PLC system words and bits be accessed within an LL984 ladder logic section?
Issue:
Trying to view system words in an LL984 section in Unity Pro.

Product Line:
Unity Pro programming software

Resolution:
No, the user would have to create an IEC section in order to view PLC system words or bits in Unity Pro.
They can be accessed through an Animation table.