Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the maximum SD Card size for the Magelis/Harmony HMIGTO and HMIGTU series Secondary Drive?
Issue
What is the maximum SD Card size for the Magelis/Harmony HMIGTO and HMIGTU series Secondary Drive?

Product Line
Magelis HMIGTO, Magelis HMIGTU

Environment
Removable Storage Media

Resolution
The Magelis/Harmony HMIGTO and HMIGTU family will support generic SD/SDHC cards up to 32GB formatted in FAT32 for the Secondary Drive slot (for Data Logging, Event & Alarm Logging, media).
Schneider Electric offers an officially validated 4GB SD Card for compatibility - the part number is HMIZSD4G