Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What can cause an motor short circuit SCF5 on an ATV61 or ATV71 drive?
Issue:
ATV61/71 SCF5 fault.

Environment:
All

Cause:
SCF5= Motor short circuit fault = Short-circuit at drive output

Resolution:
Check the motor cables connecting the drive to the motor.
Check the motor’s insulation. Using a 1,000V Megger, test the motor for windings or insulation issues.
Recheck all motor parameters. Be sure that your parameters match the information on the motor's nameplate.
Perform tests via the [1.10 DIAGNOSTICS] menu.
Run the drive open circuit (with the motor disconnected and OPL turned off) and check the drive's output terminals for balanced voltages phase to phase
Inspect and repair the drive.