Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Can you change the color of an object from the Toolchest in Vijeo Designer?
Issue:
Can you change the color of an object from the Toolchest in Vijeo Designer?

Product Line:
Vijeo Designer, Toolchest

Resolution:
No, you can not.  A work around would be to copy the object out of Vijeo Designer and paste it into a photo editing software (ex MS Paint). With the photo editing software, change the color of the object and save a new file for each of the different colors. Next, use a lamp object in Vijeo Designer that has the user defined category selected and browse the image file for ON and OFF.