Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Unity Pro V10.0 - Issue using IEC_BMDI_M function block

Facts and Changes

This IEC_BMDI_M  EF is provided in Unity Pro V10.0.
The length input parameter is not properly respected while doing bit to word copy.
If length is adjusted to 16, to copy 16 bits to 1 word, we have 16 first bits copied but not only.
It's continued doing copy up to 256bits, mean 16 words in output are written by this EF in all cases.

Causes and Fixes

A unity Pro V10 Hotfix is provided : HF0300425R.