Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How do I use the ATV71 keypad to operate my motor?
Issue:
Using the ATV71 keypad to operate a motor.

Product Line:
ATV71

Environment:
All models and serial numbers

Cause:
None

Resolution:
In the ATV71: a  function key will need to be assigned to toggle between Terminal (T) and Keypad (K).
1.  From the MAIN MENU scroll to ACCESS LEVEL, press enter
2.  Scroll down to "Expert", press enter
3.  Press ESC back to the MAIN MENU
4.  Enter on DRIVE MENU
5.  Scroll down to menu 1.6 COMMAND, press enter
6.  Scroll down to "F4 Key assignment", press enter
7.  Scroll down to "T/K", press enter
, ATV71