Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is an OSF code on an ATV12 drive?
Issue:
OSF code on an ATV12 drive.

Product Line:
ATV12

Environment:
All

Cause:
Electrical Specifications

Resolution:
OSF is a Mains overvoltage fault.  The VFD monitors the DC bus voltage.
Consider possible causes:
• Line voltage is too high:
- At drive power on only, the supply is 10% over the maximum acceptable voltage level
- Power with no run order, 20% over the maximum line supply
• Disturbed line supply and power quality issues

After removing the source of the overvoltage, cycle power to the VFD to clear the fault.  If the VFD powers up to OSF, then it has re-faulted.