Naše značky

Impact-Company-Logo-English Black-01-177x54

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the range of the nCr parameter on the ATV312 series drive?
Issue:
Programming range for the nCr (Nominal Current) Parameter

Product Line:
ATV312 series drives

Environment:

All models, All serial numbers

Cause:
Information needed for pre-purchase product selection.

Resolution:
The nCr (motor current rating) parameter can be adjusted between 25% and 150% of the nominal rating of the drive, as listed on the drive nameplate.