Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How to read the IP address of a low end M580 CPU
Issue

Where is the M580 IP address located?

Product Line
M580 low end

Environment
Unity pro 10 and lower.

Resolution

The IP address is located in two system words: %SW6 and %SW7.

%SW6 contains the two last octets of the IP address and %SW7 contains the two first octets.