Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Cannot change the FTP password for the 140NWM10000 using Web Designer.
Issue
Cannot change the FTP password for the  140NWM100000 using Web Designer.

Product Line
Ethernet Network Quantum Module

Environment
140NWM10000

Resolution
The selection for FTP password on the target security window is greyed out and not selectable.
hjkl
Due to cyber security reasons, the ability to change the FTP password for 140NWM10000 Factorycast HMI module using
Web Designer is not allowed.   Changing of the FTP password for the  140NWM10000 Factorycast HMI module must be
performed from the 'Setup' web pages.