Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Latest firmware version for the energy server Com'X 510 (Version 6.8.7)
Issue
What is the latest firmware version for the Com'X 510?
Product Line
Com'X 510
EBX510

Environment
Firmware
Resolution
As of 05/07/2024, the latest version of firmware for the Com'X 510 is v6.8.7. This version is only required for Com'X 510 devices connected to the cloud. For non-cloud connected Com'X 510 devices, upgrading to firmware 6.8.4 provides the latest features and fixes. Both firmware versions can be downloaded from the links below:

Note: Depending on the existing Com'X 510 firmware version, it must be upgraded in stages to v2.1.17, then to v3.6.3, then to the latest version. The referenced firmware files are attached to this article below.
  • If the firmware version is older than v2.1.17, it must be upgraded to v2.1.17 first.
  • If the firmware version is newer than v.2.1.17, but older than v3.6.3, it must be upgraded to v3.6.3 first.

Refer to the following article for instructions to upgrade the firmware:

Schneider Electric Česká republika

Přílohy
ComX510_v2.1.17.zip [43.63 MB]
ComX510v3-6-3_Firmware_EBX510.zip [50.38 MB]
Zjistěte více
Produkt:
Zjistěte více
Produkt: