Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Is it possible to add the alarm severity to an alarm summary column in Vijeo Designer?
Issue:
Looking for an example on how to show the alarm severity in the alarm summary.

Product Line:
Vijeo Designer (all versions)

Resolution:
Currently there is no specific column that can be added to display the alarm severity in the alarm summary. The workaround for this is to do the following:

1) Add in the alarm message the alarm severity at the beginning of the message. For ex. [1]: This alarm is active.
2) In addition, set the Alarm Summary to sort by severity as well.