Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the break down of list of last fault (LFT) communication network code numbers for the ATV61 and ATV71 drives.

Article available in these languages: Španělština

Issue:
Where can I find a list of last fault network code numbers for the ATV61 and ATV71 drives?

Product Line:
Altivar ATV61 and ATV71 with a network card installed.

Environment:
All

Cause:
They are using a network to read the last fault which shows up as a numerical code.  They need to convert the numerical code into a fault code.

Resolution:
See the attached document which shows the Last fault list codes.

Schneider Electric Česká republika

Přílohy
last fault network codes.pdf [72.24 KB]