Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Are there any IO expansions for the Magelis HMISCU HMI controller?

Issue:
Are there any IO expansions for the Magelis HMISCU HMI controller?

Product Line:
HMISCU, HMISCU8B5, HMISCU8A5, HMISCU6B5, HMISCU6A5, IO expansion, I/O expansion
EcoStruxure Machine Expert Software

Resolution:
The HMISCU does not have any IO expansion modules that connect directly to it, however now, there is a TM3 Bus Coupler Module that allows fast connectivity with TM3 I/O Modules.
The CANopen TM3 Bus Coupler - Part Number TM3BCCO connects to the embedded CANopen port on the HMISCU and is added from the Devices Tree under the CAN > CAN_Optimized node:

Add the TM3 Bus Coupler under Devices Tree > CAN > CAN_Optimized node

Underneath the TM3BC_CANopen node, TM3 Digital and Analog I/O Modules can be added:
Add TM3 I/O Modules under the TM3BC_CANopen node

From there, the TM3 I/O Modules can be configured and symbols can be mapped:
Configure and map the TM3 I/O Module

Also see the Catalog for TM3 Expansion IO Modules .



[Legacy Information]
Before the addition of the TM3 Bus Coupler in EcoStruxure Machine Expert, the previous options would have been to use:

  1. Advantys OTB island
  2. Advantys STB island
  3. use a small PLC (M221) with a Magelis (HMISTU) instead of the HMISCU.

There are three Advantys OTB options (they differ in terms of connectivity to the PLC):
  1. OTB1C0DM9LP - CANopen
  2. OTB1S0DM9LP - Modbus
  3. OTB1E0DM9LP - Ethernet MB-TCP/IP
Variants of the TM2 I/O modules can be added to the Advantys OTB island.
The OTB1C0DM9LP (CANopen) version's configuration software is integrated into SoMachine v3.1 and higher.
Example Digital I/O TM2 Module that can be used:
TM2DMM8DRT - Discrete I/O module M238 - 4 inputs 24 V DC - 4 outputs relay- 1 terminal block
Example Analog I/O TM2 Modules that can be used are:
TM2AMM6HT - Analog input/output module M238 - 4 inputs voltage/current high level - 2 output
Here is a link to the OTB and TM2 product range:

What distributed I/O network interface modules are available for Advantys OTB ?