Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How do I connect my PC to my Altivar drive?
Issue:
Is there an option for the Altivar drives to connect using a RS232 connection?

Product Line:
Alitivar

Environment:
All

Cause:
Product Selection & Services

Resolution
No, converter options for RS232 to RJ45. There is a cable available for a RJ45 to USB part number TCSMCNAM3M002P USB to RJ45
adaptor
For use in connecting to a PC with a USB port
Advantys™ OTB,
Altistart™ motor starters,
Altivar series including
HMI, Altivar controller