Naše značky

Impact-Company-Logo-English Black-01-177x54

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the DC bus level at which the Brake resistor engages for the ATV312 Drives?
Issue:
DC bus level at which the Brake resistor engages for the ATV312 drives

Product line:
ATV312, Altivar 312

Environment:
all

Cause:
n/a

Resolution:
The internal transistor will output to a Brake resistor at the following voltage levels:

For 200-240V drives, the DC bus level is 379V
For 380-480V drives, the DC bus level is 792V
For 575V drives, the DC bus level is 948V