Prohledejte časté dotazy
What is the replacement to the Modbus Plus PCI-85 I/F card Part# 416NHM30030(A) and 416NHM30032(A)?
Title
Modbus Plus PCI-85 I/F card Part# 416NHM30030(A) and 416NHM30032(A) Replacement
Issue
The replacement part number for the Modbus Plus PCI-85 I/F card Part# 416NHM30030(A) and 416NHM30032(A)?
Product Line
Modbus Plus
Resolution
The new Modbus Plus Express (PCIe) Part# 416NHM30042A card support 2 Modbus+ ports and can operate in a single or redundant cabling architecture. As a consequence, it can replace the previous 416NHM30030(A) and 416NHM30032(A) PCI standard cards.
Modbus Plus PCI-85 I/F card Part# 416NHM30030(A) and 416NHM30032(A) Replacement
Issue
The replacement part number for the Modbus Plus PCI-85 I/F card Part# 416NHM30030(A) and 416NHM30032(A)?
Product Line
Modbus Plus
Resolution
The new Modbus Plus Express (PCIe) Part# 416NHM30042A card support 2 Modbus+ ports and can operate in a single or redundant cabling architecture. As a consequence, it can replace the previous 416NHM30030(A) and 416NHM30032(A) PCI standard cards.
Publikováno pro:Schneider Electric Česká republika
Zjistěte více
Řada:
Zjistěte více
Řada: