Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Is there a cost for the Vijeo Designer Data Manager tool?
Issue:
Is there a cost for the Vijeo Designer Data Manager tool?

Product Line:
Vijeo Designer (all versions)

Resolution:
No, the Vijeo Deisgner Data Manger tool is intended for free distribution to end users of Magelis HMIs running Vijeo Designer Runtime. The tool is to be used to retrieve data stored on the HMI. It is typical that the end-user has not purchased Vijeo Designer. Contact technical support for a download link for the tool.