Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What is the replacement for the Magelis XBTGT7340?
Issue:
The Magelis XBTGT7340 is no longer in production. What is its replacement?

Product Line:
Magelis HMI, Magelis XBTGT series

Resolution:
The replacement for the Magelis XBTGT7340 can be one of two models depending on the need for video or multi-media support.
If video support is not required, use the combination: HMIG3U (Premium BOX CPU module) together with the HMIDT732 (15" touchscreen that snaps onto the front of the CPU module).
If video support is required, use the combination: HMIG5U2 (Open BOX CPU module) together with the HMIDT732 (15" touchscreen that snaps onto the front of the CPU module).

NOTE: The old application designed for the XBTGT7340 can be used with either the HMIG3U or HMIG5U2 with little modification. Generally we only need to switch the Target Type and Target Model. In rare occasions, some I/O driver settings may need to be updated.

The required software to program the HMIG3U is Vijeo Designer 6.2 SP5 or greater. Please update the software. The latest service pack for Vijeo Designer 6.2 is SP12 (Service Pack 12).