Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What may cause the New Variables from Equipment to be empty when linking the Vijeo Designer V6.2 variables to Unity Pro v?
When linking to a Unity Pro XVM or STU files, check that the IEC61131 box is checked in the Modbus Equipment driver configuration window.
Also check that there are no variable filters turned on. In addition, also check that the Unity project is built prior to export of the XVM file.