Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Does the Generic PC Series Target with Vijeo Designer Runtime support Web Gate?
Issue:
Looking for information regarding Web Gate and the Generic Windows PC series in Vijeo Designer

Product Line:
Vijeo Designer (all versions)

Resolution:
Yes, the Generic PC Series Target in Vijeo Designer supports the Web server and Web gate feature. The platform is exactly the same as an IPC which also supports all the features available in Vijeo Designer.