Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
EGX150 serial communication cable

Issue
User is trying to purchase a cable to wire serial communication to EGX150 (Link150) to downstream devices through its RJ45 serial port

Product Line
EGX150 (Link150)

Environment
Serial communication

Resolution
Part# VW3A8306d30

This cable is for Modbus serial link 1xRJ45, free wires at the other end. 3m length

The correspondence between the wire colors of cable VW3A8306D30 and the pin numbers of the RJ45 socket is as follows:

Wire diagram

For EGX150 wiring connection to serial RS485, please reference

https://www.se.com/us/en/faqs/FA323145/

RS485 wiring