Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Does the M580 Hot Standby CPU's support %SW60 - 65 and %SW69 ?
No. These words are dedicated to the Unity Quantum HSBY solution.
The M580 uses a DDT (Device Data Type) which is automatically created when selecting an M580 HSBY processor in Control Expert (formerly Unity Pro)..

The DDT is named ECPU_HSBY_1. All of the functionality and status information offered by %SW60 - 65 for Quantum HSBY is made
available through this DDT for M580 HSBY user.