Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Is there a 120V control option card available for the ATV630 Process drives?

Issue:
Is there a 120V control option card available for the ATV630?

Product Line:
ATV630, ATV Process

Resolution:
A 120VAC input adapter card is not available for the process drives.
Consider an interposing relay for each digital input used.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.