Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What does 410 at the end of the ATV312 part number mean? Example: ATV312HD11N4410.
Issue:
"410" Suffix on the ATV312HD11N4410.

Product Line:
ATV312

Environment:
Part numbers ending in 410

Cause:
N/A

Resolution:
This is a custom modified version of the ATV312 that is only sold to the customer who had it customized.
A standard ATV312 will not work in it's place.  It has to be ordered through the OEM.