Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Do the ATV630 and ATV930 Process Drives come with a keypad?
Issue:
ATV630 and ATV930 Process Drives come with a keypad.

Product Line:
Altivar Process 630, Altivar Process 930

Environment:
All part numbers

Cause:
Customer wants to know if the keypad is included or needs to be ordered separately.

Resolution:
YES, the drives come with a keypad.
The keypad can also be ordered separately, if needed, part number is VW3A1111.