Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
The Edit button dissapears when trying to change IP Address on my PM5000 series meter

Issue:

When attempting to change the IP Address of a PM5000, the Edit button dissapears when scrolling to the IP Address or Subnet mask.

Product Line:
PM5000 Series

Environment:
Meter Front Display

Cause:
This is caused when the IP Method is set to something other than "Stored". When set to Stored, the IP Address becomes "Static" and therefore configurable on the meter. The other options (Default, DHCP, BOOTP) do not allow the IP to manually be configured as the IP is set by the network.

Resolution:
In order to be able to change the IP Address from the front panel of the PM5000 series, change the IP Method to "Stored".