Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
How do I turn on the Multi-Pump function on the Altivar 630 Process drive?
Issue:
Multi-Pump function on the Altivar 630 Process drive

Product Line:
Altivar 600 Process Drive

Environment:
All serial numbers for Altivar 600 Process Drive

Cause:
N/A

Resolution:
Turn on Macro Configuration to either (Booster Control or Level Control)
[Complete settings] [Macro configuration]

[Complete settings] [Pump functions] [Booster control] [System architecture]


[Pump System Architecture] MPSA would have to be turn on or set to [Single Drive] VNDOL or [Multi Drive]
Firmware version up to 1.5 will give you choice of Single Drive only. Version 1.6 and over will give you choice of Single and Multi Drive.

Once [Pump System Architecture] MPSA has been configured then configure [Nb Of Pumps] MPPN
(max. 6 pumps)


To configure each individual pumps,
[Complete settings] [Pump functions] [Booster control] [System architecture] [Pumps
configuration]


See the attached document for additional programming assistance.

Schneider Electric Česká republika

Přílohy
ATV6xx_Programming_Manual_EN_EAV64318_03 (Multi-Pump).pdf [373.56 KB]