Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Are the ION7400, PM8000 and PM5000 Dual Ethernet Ports Protocol Agnostic?
Issue
Customer wants to use different protocol for each Ethernet port on the ION7400, PM8000 or PM5000 meter

Product
ION7400 series
PM8000 series
PM5000 series with dual Ethernet ports

Environment
Networking

Resolution
The ION7400, PM8000 and PM5000 meters with dual Ethernet ports have an internal Ethernet switch that is protocol Agnostic.
Each port can be used for different protocols such as ION and Modbus on ION7400 and PM8000, or Modbus and BACnet on PM5000.