Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
What causes the error: Mismatch Type with reference variables in Vijeo Designer v6.2?
Issue:
What causes the error: Mismatch Type with reference variables in Vijeo Designer?

Product Line:
Vijeo Designer

Resolution:
The issue could be that the reference tag was referencing itself initially and that is not valid.  Or the reference tag is referencing a different datatype.