Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Is there an EDS file available for the M221?
Issue:
Is there an EDS file available for the M221 Ethernet/IP communications?

Product Line:
TM221

Resolution:
Yes, the EDS file for the M221 is located in the installation path of Somachine Basic \Firmwares & PostConfiguration\M221

Please note that EDS file will need to be modified to match your settings in the Somachine Basic for Ethernet/IP configuration.
Attached is the EDS file and the instructions to modify the EDS file.

Schneider Electric Česká republika

Přílohy
Instruction for EDS File Modification.pdf [68.42 KB]
M221 EDS file from SoMachine v1.4.zip [64.81 KB]