ATV600/ATV900 has to be in the same IP range as the PC. For access to webserver the drive IP address has to be entered to any webrowser (Internet Explorer, Mozzila Firefox, Opera, Chrome...). User name is "ADMIN". Deafault password is unique for every drive (required by Achilles L2 certification) and can be found in menu My Preferences (8) - Webserver (8.7) - Webserver default pasword. If additional ethernet communication card is used, it has another default password, which is also displayed in this menu. Password are displayed after the drive is connected to the network. Password has to be changed after firs log in (required by Achilles L2 certification).
Note: Drives with old firmware - up to 1.3 for ATV600 and up to 1.1 for ATV900 has default user name "admin" and default password "ADMIN". These drives do not fulfill Achilles L2 requirements.