Naše značky

Vítejte na internetových stránkách společnosti Schneider Electric

Vítejte na našich internetových stránkách.
		
Jak vám dnes můžeme pomoci?
Are lugs available as a replacement part for high horsepower ATV600 / ATV900 series Process Drives?

Issue:
Availability of lugs as a replacement part for high horsepower ATV600 / ATV900 series Process Drives

Product Line:

ATV6xx, ATV9xx

Environment:
All


Cause:

Customer needs to install or replace lugs


Resolution:

We do not offer lugs for the ATV600/ ATV900 series drives.  Bare terminals are available on the drive so that the customer can best choose the lugs to match the wiring they are using. We would suggest contacting Thomas & Betts, Burndy or Illsco for lugs.

The open style ATV6XX and/or ATV9XX has ring terminals that indicates that lug kits do not come with the high horse power units.

If it's ordered as part of an ATV660 enclosure, MCC package or Altivar outdoor they would probably be included, but not with an open style Drive that has a high horse power rating.